Module Use in Applications (ZN-T Setpoint Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The application System Selection trees use the individual modules in this group using the names in Table 1.

Table 1. ZN-T Setpoint Determination Uses in Application System Selection Trees

Module Instance Name

Applications

ZN-T Setpoint Determination

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU Rooftop Unit Applications

Fan Coil Applications

Heat Pump Applications

Unit Ventilator Applications

VAV Single Duct Applications

VAV Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.