This module determines the minimum deck flow setpoints (heating and cooling) according to the occupied and warmupcooldown conditions within a VAV dual duct application. The module accepts Occupancy, WarmupCooldown modes, and flow setpoints. The module outputs the minimum deck flows. During conditions of Standby, the unoccupied flow setpoints are issued. During conditions of Unoccupied, the unoccupied flow setpoints are also issued unless there is a warmup/cooldown mode. During conditions of Occupied or Bypass, the occupied flow setpoints are issued.
You can view and modify the modules in this group’s logic.