The following table describes the attributes used by the Temperature Request Determination module.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
CD Percent |
Represents the cooling damper command. |
0% open |
|
Cooling Request |
G |
Indicates the output of the module:
|
0 |
Cooling Setpoint |
Indicates the maximum damper command that initiates a decrease in supply temperature. |
95% open |
|
Differential |
Indicates the required reduction in damper command before pressure request is no longer required. |
10% |
|
HD Percent |
Represents the heating damper command. |
0% open |
|
Heating Request |
Indicates output of module:
|
0 |
|
Heating Setpoint |
Indicates the maximum damper command that initiates an increase in supply temperature. |
95% open |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)