Module Use in Applications (Damper Minimum Position Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in Table 1.

Table 1. Damper Minimum Position Determination Uses in Application System Selection Trees

Module Instance Name

Applications

Damper Minimum Position Determination

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

AHU Multizone (Mixed Air Dual Duct) Applications

AHU Rooftop Unit Applications

Min Position Determination

Heat Pump Applications

Unit Ventilator Applications

To see a module's connections and how modules interact with it, view the Connections table.