Attributes (Damper Minimum Position Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
Table 1 describes the attributes used by the Damper Minimum Position Determination modules.

Table 1. Damper Minimum Position Determination Attributes

Name

Type 1

Description

Default Value

Occupancy

 

Current Occupancy status of the unit.

Occupied

Set Name: Occ Effective

Occ Minimum OA Percent

 

Contains the desired damper minimum position during occupied or bypass mode.

10.0%

Minimum OA Position

G, V

Minimum damper position.

0.0%

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)