Attributes (Equipment Count) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by this module:

Table 1. Equipment Count Attributes

Name

Type

Description

Default Value

Fan State

 

Indicates if more fans are ON than the defined minimum number of running devices using a Boolean value.

False

Fan Status

 

Indicates if more fans are ON than the defined minimum number of running devices using an enum output.

Off

Set Name: Off/On

Input n (where n is 1-16)

 

Provides the Binary status of each fan.

Off

Set Name: Off/On

Minimum Running Devices

G

Indicates the comparison threshold, where less than this number of fans is not considered ON for overall status.

1

Number of Devices Running

 

Indicates the number of inputs with a value of ON.

0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)