This module is responsible for determining the required minimum flow setpoint for two pipe plants. This module accepts the inputs listed below. The module outputs either the cooling minimum flow or the heating minimum flow depending on the plant mode. It is implemented as a standard Control Activity.