Minimum Flow Calculation - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Minimum Flow Calculation module provides a minimum flow value based on the number of running devices. This module provides a float output. Based on the inputs, the module sets the Output equal to the Min Flow or the sum of the devices currently running, whichever is larger.