Module Use in Applications (Flow Sum Calculation) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in Table 1.

Table 1. Flow Sum Calculation Uses in Application System Selection Trees

Module Instance Name

Applications

Calculate Supply Flow

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

Calculate Supply Flow Setpoint

VAV Dual Duct Applications

VAV Subordinate Dual Duct Applications

Discharge Flow Determination

AHU Mixed Air Dual Duct Applications

AHU 100% Outdoor Air Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.