Table 1 describes the attributes used by the Flow Differential Calculation module.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
CD-F, HD-F, or FLOW (Calculated Flow) |
G, V |
Contains the result of the subtraction with reliability. |
Display Units: l/s, cfm |
Contributing Flow |
Measured flow to be subtracted from the Total Flow. |
0 l/s, 0 cfm |
|
Total Flow |
Measured total flow. |
0 l/s, 0 cfm |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)