Attributes (Unocc Heating Fan Lockout) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

Table 1 describes the attributes used by the Unocc Heating Fan Lockout module.

Table 1. Unoccupied Heating Fan Lockout Attributes

Name

Type 1

Description

Default Value

Heating isAvailable

 

Provides a network input used to enable or disable heating.

False

Heating Required

 

Indicates whether there is a need for heating.

True

Occupancy

 

Indicates the effective occupancy command.

Occupied

Set Name: Occ Effective

Preheat isAvailable

 

Provides a network input used to enable or disable the preheat functionality.

False

Present Value

 

Indicates the current status of the device availability. The Present Value is True when the device is available and False when the device is not available.

False

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)