WarmupCooldown Determination - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

This module determines the effective WarmupCooldown status for single duct VAV applications by evaluating the Network Input and the automatic Warmup mode based on the supply air temperature. The module issues a warmup status ANY TIME the SA-T (Supply Air Temperature)meets the requirements necessary for warmup (that is, both SA-T and ZN-T are reliable and SA-T > [ZN-T+Differential]). If both SA-T and ZN-T are reliable and the SA-T is not warm enough to trigger warmup, the WC-C (WarmupCooldown) network input is not allowed to force warmup (remains in Normal). The module state output is the effective WarmupCooldown mode for the application.

You can view and modify the modules in this group’s logic.