Table 1 describes the attributes used by the Status Alarm Determination module.
Name |
Description |
Default Value |
---|---|---|
Alarm |
Indicates the current alarm status of the device. |
Normal Set Name: Normal/Alarm |
Command |
Indicates the current command to the device. |
Off Set Name: Off/On |
Delay |
Delay (time period) allowed to elapse after the device starts and before it indicates a fault. |
30 seconds |
Flow Status |
Indicates the current status of the device. If Failsoft is True, the switch is set to Off when the input is not Reliable. |
Off Set Name: Off/On |
Status |
Indicates the current effective status of the device. When True, the device is commanded on and the Flow Status is on. This value is False when the Flow Status input is off. |
False See Primary States (Status Alarm Determination). |