Primary States (Staged Device Enable Determination Series) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
  • False: Conditions are not appropriate to allow staged devices to operate.

  • True: Conditions are appropriate to allow staged devices to operate.

  • Fault: Conditions are not appropriate to allow staged devices to operate.