Module Use in Applications (Staged Device Enable Determination Series) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use individual modules in this group using the names in Table 1.

Table 1. Staged Device Enable Determination Series Uses in Application System

Module Instance Name

Applications

Staged Device Enable Determination Series

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.