Attributes (Staged Device Enable Determination Series) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

Table 1 describes the attributes used by the Staged Device Enable Determination Series module.

Table 1. Staged Device Enable Determination Series Attributes

Name

Type 1

Description

Default Value

Fan Mode

 

Last command sent to the fan.

Off

Set Name: Off/On

STGDEV-MINFLOW (Staged Device Min Flow)

 

Minimum required flow that must be reached (without the fan being commanded on) before the system issues a True.

100 l/s, 200 cfm

STGDEV-STATE (State)

G, V

Current effective status indicating whether the staged device should be enabled or disabled.

Enable

Set Name: False/True/Fault

Supply Flow

 

Indicated the current supply airflow rate.

0 l/s, 0 cfm

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)