Module Use in Applications (Staged Device Enable Determination Parallel) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in Table 1.

Table 1. Staged Device Enable Determination Parallel Uses in Application System

Module Instance Name

Applications

Staged Device Enable Determination Parallel

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.