Staged Device Enable Determination Parallel - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

This module generates a True, False, or Fault state to indicate to a parallel staged device that the airflow requirements have been met. For a parallel device (a parallel fan in a single duct VAV box application), the only requirement to enable the device is that the fan is commanded on.

You can view and modify the modules in this group’s logic.