Primary States (Flow Status Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
  • False: The Airflow Proving Switch is Off and the Fan Mode is Off or has been On for less than the Delay time.

  • True: The Airflow Proving Switch is On and the Fan Mode is On.

  • Fault: The Airflow Proving Switch is Off and the Fan Mode has been On for at least the Delay time.