Module Use in Applications (Dual Fan Speed High Select) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Dual Fan Speed High Select Uses in Application System Selection Trees

Module Instance Name

Applications

Dual Fan Speed High Select

AHU Mixed Air Single Duct Applications

AHU100% Outdoor Air Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.