The following table describes the attributes used by the Dual Fan Speed High Select modules.
Name 1 |
Type 2 |
Description |
Default Value |
---|---|---|---|
Input 1 |
Indicates the float variable that is compared to other inputs. |
0 Display Units: None |
|
Input 2 |
Indicates the float variable that is compared to other inputs. |
0 Display Units: None |
|
Fan Percent Cmd |
G |
Indicates the result of the high select. |
0.0 Display Units: None |
1 Attributes apply to all the modules within this category.
2 B: BACnet Exposed Parameter, C: Configuration Mode Only, G: Default Element (Generated State, if applicable), SC: Simulation and Commissioning Modes Only, V: Calculated Value (Outputs)