Attributes (Dual Fan Command OR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The following table describes the attributes used by the Dual Fan Command OR modules.

Table 1. Dual Fan Command OR Attributes

Name

Type 1

Description

Default Value

Command

 

This input represents the command being sent to the first device.

Off

Set Name: Off/On

Command 2

 

This input represents the command being sent to the second device.

Off

Set Name: Off/On

Output

G

This is the result of the OR operation.

Off

Set Name: Off/On

1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)