Dual Fan Command OR - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Dual Fan Command OR Module provides the ability to OR the inputs to the module and passes the result to the output. This module is implemented as a control activity.

You can view and modify the modules in this group’s logic.

Figure 1. Dual Fan Command OR Logic