The following table describes the attributes used by the Analog Status Determination module.
Name |
Type 1 | Description | Default Value |
---|---|---|---|
Fan State | Indicates the calculated status of the fan array using a Boolean format:
|
False | |
Fan Status | Indicates the calculated status of the fan array using the off/on enum set. | Off | |
Minimum Running Devices | Indicates the minimum number of devices that constitute fan operation. | 8 | |
Number of Devices (input) | Indicates maximum number of devices wired to the single input. | 8 | |
Number of Devices (output) | Indicates calculated number of operating devices. | 9 | |
Resistance 1 | Indicates current resistance measured by the analog input. | 100 | |
Resistance per Fan | Indicates number of Ohms each fan status reduces the measured resistance by. | 100 |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)