Attributes (Subtract) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by the Subtract modules:

Table 1. Subtract Attributes

Name

Type 1

Description

Default Value

CHWTEMP-DIFF or CHWFLOW-DIFF [Output (Float)]

V

Indicates the differential of Input 2 subtracted from Input 1.

0

Input 1

 

Indicates the floating variable from which Input 2 is subtracted.

0

Input 2

 

Indicates the variable that is subtracted from Input 1.

0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)