Module Use in Applications (Flow Direction Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Flow Direction Determination Uses in Application System Selection Trees

Module Instance Name

Application

Decouple Flow Loop Determination

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.