The following table describes the attributes used by this module:
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Flow Direction |
This input is the direction of the flow. It is used when a directional flow BI is included in the system. |
Normal Set Name: Polarity |
|
Flow Input |
This input is the measured flow through the decoupled flow loop. This input may or may not have direction associated with it. |
0.0 gpm, 0.0 L/s Display Precision: 1s |
|
Present Value |
This output is the decoupled flow merged with flow direction. A negative flow represents flow in the reverse direction. |
0.0 gpm, 0.0 L/s Display Precision: 1s |
1 B - BACnet Exposed Parameter, C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)