The following table describes the attributes used by the Device Alarm modules:
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Input n |
Indicates the inputs to this module (where n is 1-8). |
Normal Set Name: Normal/Alarm |
|
Maintenance Switch |
G |
Provides the result of the OR operation and any latching, as translated into the Disable/Enable value of the Maintenance Switch. |
Enable Set Name: Disable/Enable |
Output |
Provides the result of the OR operation and any latching. |
Normal Set Name: Normal/Alarm |
|
Reset n |
Indicates the inputs used to set the Output back to normal when Setup n is Manual (where n is 1-8). |
Off Set Name: Off/Reset |
|
Setup n |
Indicates the latching action for the specific input (where n is 1-8). When Setup n is Automatic, the Output is Alarm if the associated input is Alarm. If all inputs and Cascaded OR Input are Normal, the Output is Normal. When Setup is Manual, the Output is Alarm if the associated input is Alarm. If all inputs and Cascaded OR Input are Normal and Reset is set to Reset, the Output is set to Normal. |
Automatic Set Name: Reset Type |