Module Use in Applications (Chiller Forced Upstage) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Chiller Forced Upstage Uses in Application System Selection Trees

Module Instance Name

Applications

Chiller Forced Upstage

Central Cooling with Optimization Applications

To see a module's connections and how modules interact with it, view the Connections table.