The application System Selection trees use the individual modules in this group using the names in the following table.
Module Instance Name |
Application |
---|---|
Capacity Calculation Amp XX (Where XX is 01-08) |
|
Capacity Calculation Pct FLA X (Where XX is 01-08) |
|
Chiller Load Total Calc Amps |
|
Chiller Load Total Calc Pct Amps |
|
CHW Pump Capacity Check X (Where X is 1-8) |
|
CW Pump Capacity Check X (Where X is 1-8) |
To see a module's connections and how modules interact with it, view the Connections table.