Attributes (CW Temperature Diff Calc) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The following table describes the attributes used by the CW Temperature Diff Calc modules:

Table 1. CW Temperature Diff Calc Attributes

Name

Type 1

Description

Default Value

ChlrX CW Entering Temp (Where X Is 1-8)

 

Indicates the entering condenser water temperature for the associated chiller.

0 °C, 0 °F

ChlrX CW Leaving Temp (Where X Is 1-8)

 

Indicates the leaving condenser water temperature for the associated chiller.

0 °C, 0 °F

Command X (Where X Is 1-8)

 

Indicates the current command of the associated chiller or pump.

Off

Set Name: Off/On

Output

G

Provides the result of the module’s calculation, which is the largest CW differential value output.

0.0

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)