Module Use in Applications (Alarm OR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The application System Selection trees use individual modules in this group using the names in the following table.

Table 1. Alarm OR Uses in Application System Selection Trees

Module Instance Name

Applications

Fire Damper Alarm OR

All Air Handling Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.