Attributes (Alarm OR) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The following table describes the attributes used by the Alarm OR modules.

Table 1. Alarm OR Attributes

Name

Type 1

Description

Default Value

Alarm

 

Provides a Boolean output value that indicates if any input is in Alarm.

False

Alarm - OR

G, V

Indicates the output of the module. When any input is in Alarm, this output is in Alarm.

Normal

Set Name: Normal/Alarm

Cascaded OR Input

 

Provides, as an input, the Cascaded OR Alarm from an additional module.

Normal

Set Name: Normal/Alarm

Device X Alarm (Where X is 1-8)

 

Provides, as an input, the binary alarm for up to 8 devices.

Normal

Set Name: Normal/Alarm

Normal

V

Provides a Boolean output value that indicates all inputs are Normal.

False

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)