Attributes (Alarm AND) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The following table describes the attributes used by the Alarm AND modules.

Table 1. Alarm AND Attributes

Name

Type 1

Description

Default Value

Alarm

 

Provides a Boolean output value that is true if ALL inputs are in Alarm.

False

Alarm - AND

G, V

Indicates the output of the module. When all inputs are in Alarm, this output is in Alarm.

Normal

Set Name: Normal/Alarm

Cascaded AND Input

 

Provides, as an input, the Cascaded AND Alarm from an additional module.

Normal

Set Name: Normal/Alarm

Device X Alarm (Where X is 1-8)

 

Provides, as an input, the binary alarm for up to 8 devices.

Normal

Set Name: Normal/Alarm

Normal

V

Provides a Boolean output value that is true if any input is Normal.

False

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)