Alarm AND - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Alarm AND module examines up to nine Enum inputs and provides AND logic, where all inputs must be in Alarm for the Alarm AND output to be in Alarm. This module provides a Boolean output that indicates when any input is Normal, and a Boolean output that indicates when all inputs are Alarm. The module accepts eight Normal/Alarm inputs and a cascaded input in cases where you need more than eight inputs, and has outputs for any input Normal, all inputs Alarm, and an alarm output.

This module is implemented as a Control Activity.

You can view and modify the modules in this group’s logic.

Figure 1. Alarm AND Logic