About this task
The Display Order property organizes how components appear within the UI. For example, a series of components nested in a tab container is displayed from left to right, such that the component appearing at the top of the list in the custom configuration panel is located as the far left tab within the UI. In a vertical orientation container, the component at the top of the list appears at the top of the container. In a horizontal orientation container, the component at the top of the Display Order appears on the far left of the container in the UI.
Note: You cannot change the order of the Classic View or Simple View components.
Procedure
- Click Settings and select Perspective Management. The Perspective Management window appears.
- In the left pane, select a perspective or container with subcomponents to reorder. The right pane populates with the available items to reorder in the Display Order box.
- Select an item and click the up arrow () or down arrow () to change the display order.
- Click Apply.
- Click Close.