Specialized Widgets - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The following fields appear for specialized widgets: Advanced Data, BACnet Exposed, Connections, Local Display, Logic View, Parameters, State Tables, and System Selection Information.

Table 1. Specialized Widgets
Field Description
Name Indicates the name of the widget. This name appears within the UI, and can be changed, if you wish.
Data Criteria Type Only Not Applicable.
Visible Indicates if the widget appears within the UI.