The Mass Edit dialog box allows you to filter and mass edit BACnet Exposed and hardware points.
Screen Area | Description |
---|---|
Show All | Shows all points. |
Show BACnet Exposed | Shows only those points that are BACnet Exposed. |
Show Hardware | Shows control points, sensors, miscellaneous points, and edited rows. |
Show BACnet Exposed Duplicates | Shows points that have duplicates. |
Show Edited Values | Shows points that have edited values. |
Filter | Use to filter your results based on partial or full search terms. |
BACnet Exposed | Use to change the BACnet Exposed property of the point. To select or deselect all entries, right-click the heading of this column. |
User Name |
Use to type a name for the point. Note: If this field is blank, the Standard Name is used.
|
Description | Use to enter a description for the point. |
Long Name | Displays the full name of the point. |
Standard Name | Displays a Johnson Controls standard name for the module. |
OK | Saves changes and closes the dialog box. |
Cancel | Discards changes and closes the dialog box. |