The following table provides information on selections found in the details data custom configuration panel.
Field | Description |
---|---|
Name |
Indicates the name that appears within the perspective UI. |
Description |
When the Details Data widget is located within a Tab container, the Description text appears as a tooltip within the UI when you hover over the tab. |
Data Criteria Type |
BACoid is only selection. |
Visible | Indicates if the widget appears within the UI. |
Settings - Show All | When selected, shows all points within application. When cleared, shows only BACnet Exposed points.
Note: This attribute appears only when you have an application open.
|
Expansion Level | Indicates the level of details that appear within the tree (1 to 5).
Note: This attribute appears only when you have an application open.
|
Filter | Provides a text box to search the selection tree based on the node name. The search results include the matching node and its ancestors. |
Manual Entry - Object Identifier | Indicates the object type and Object ID of the associated BACoid. |