Logic View - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

The Logic View widget functionality is identical to the previous release's Logic tab. This widget does not need to appear as a tab and can be located anywhere within the UI. For more information, see Logic Tab.