UI Column - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The UI Column data criteria type is supported by the Table Data widget only. This data criteria type allows you to select a group of modules or points from a list of UI column options:
  • Control Points
  • Miscellaneous Inputs
  • Miscellaneous Outputs
  • Network Inputs
  • Network Outputs
  • Output Controllers
  • Sensors
  • Setpoint Determination
  • State Generation
  • State Selector

Each UI Column data criteria Table Data widget can support one or multiple categories of information (such as Network Inputs only, or all types of Inputs—Sensors, Miscellaneous Inputs, and Network Inputs).