Data Criteria - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
Each widget has a data criteria type, which may be configurable or not configurable depending on the widget. Specialized widgets, such as Advanced Data, Logic View, Parameters, BACnet Exposed, Connections, Details Data, Local Display, State Tables, and System Selection Information, do not have configurable data criteria. The data criteria for these widgets displays only as Not Applicable. Configurable widgets include Table Data and Details Data widgets. The following sections provide more information on configurable data criteria.