Orientation - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

The Orientation container specifies the orientation of components (vertical or horizontal). For example, in the Classic View, the Network Inputs, Inputs, and Miscellaneous components are arranged in a vertical orientation, where they appear stacked vertically. However, within the Control tab, the module categories are arranged horizontally, or next to each other. See Figure 2 for an example of Vertical and Horizontal orientation.

The following two figures illustrate the Orientation property. Figure 1 shows two Table Data widgets within a Vertical Orientation container and two Table Data widgets within a Horizontal Orientation as the configuration appears within the Perspectives tab of the Perspective Management dialog box. Figure 2 shows how these widgets appear in the UI.

Figure 1. Perspective Tree Example Orientation Container Configuration

Figure 2. Perspective View of Vertically and Horizontally Oriented Table Data Widgets