When you build a perspective, containers allow you to organize the content according to specific properties. Container types include Frame, Orientation, and Tab. Each container type can be added individually. In addition, after adding a container, you can change the type to another type of container, such as switching an Orientation container to a Tab container.
Icon | Description | Properties |
---|---|---|
Indicates a Frame container, which can only be added at the root level. |
Orientation |
|
|
Indicates an Orientation container, which can be vertical or horizontal. |
Orientation Resizable Visible |
Indicates a Tab container, which can be positioned in various locations of the UI. |
Position Visible |