Associated Perspectives - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02

Perspectives are associated with the applications provided by the tool, such as VAV, Central Cooling Plants, Air Handling Units, and so on. The Associated Perspectives view on the System Configurations tab of the Perspective Management screen allows you to edit the associated perspectives for your applications. See Configuring Associated Perspectives Per Application and Configuring Associated Perspectives for All Applications. See Applications for more information on applications provided by the tool.