Systems Not Suited for PRAC+ - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
When PRAC+ is applied to certain systems for which it was not designed, the performance is less than ideal. PRAC+ was designed for the majority of linear first-order plus delay systems. While most mechanical systems that are encountered in the field match this description, for other systems, it may be desirable to turn off PRAC+ and manually tune the PID. Examples of these systems include: