Viewing and Adding Unmapped Objects - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Brand
Johnson Controls
Metasys
Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
Language
English

About this task

Certain objects are not always exposed within the CCT UI. To expose the objects for viewing, follow these steps:

Procedure

  1. In the CCT UI, right-click the output controller and select Logic View. The Logic View appears.
  2. Select Control Mode. This view shows the flow of the PID.
  3. Right-click the PID and select Expose Ports > For BACnet. See Figure 1.
    Figure 1. Expose Ports for BACnet

  4. To map objects, see Adding Objects Manually or Adding Objects Using Auto-Discovery.