Output Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0
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
The outputs module category lists the outputs defined for the system. Outputs are the points that get connected to an actual device, representing a physical hardware point in the system. Outputs can also represent a point associated with an output. Outputs send data to hardware output points of a device. Outputs may be connected to the Network Sensor, as well as Analog Inputs, Analog Outputs, Binary Inputs, and Binary Outputs.

See the following sections for information:

See the Upgrading System Files section for a list and description of the module and System Selection changes that were made since the last release of the tool.