Input |
Behavior When Input Is Not Reliable |
---|---|
Process Variable |
If the State is Control, the PID skips execution and holds its output at its last value. |
Reset Input |
The last Reliable value is used as the input. |