Primary States (Sideloop Interlock Binary to Binary) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 16.0

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
16.0
Revision date
2023-10-02
  • Off: The Present Value is set to Off.

  • On: The Present Value is set to On.

  • Control: If the Input is On and all timers are satisfied, the Present Value is set to On. If the input is Off and all timers are satisfied, the Present Value is set to Off.